{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Which products can I use with the TeSys Quickfit system?

The TeSys Deca range of contactors and GV2ME circuit breakers with spring terminals are compatible with TeSys Quickfit.

To specify a contactor with spring terminals, a 3 is added to the part number before the coil voltage. For example, an 18a AC-3 rated contactor with a 110v AC coil would be LC1D18F7. With spring terminals, this part number is LC1D183F7.

Similarly, with the GV2ME motor circuit breakers, a 3 is added at the end of the part number. The standard 2.5-4a version of this would be part number GV2ME08. With spring terminals, this part number is GV2ME083.

Further information on the TeSys Quickfit system can be found by clicking the link below.
TeSys Quickfit - www.se.com/uk/en/product-range/699-tesys-quickfit

Schneider Electric UK