{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What replacement enclosures are available for the TeSys LG and LJ enclosed Starters?
Empty enclosure for LG1 or LG7 or LG8 or LJ7 or LJ8 are available with the following references:
  • DE1KS217A04 : without pushbutton.
  • DE1KS217A06 : with start stop.
  • DE1KS217A29 : with padlocking (without button).
  • DE1KS217A06A29 : with start stop and padlocking.
We have previously sold these variations, but they are now obsolete:
  • DE1KS217A37 : with emergency stop (without button).
  • DE1KS217A29A39 : with padlocking, emergency stop (without button).
  • DE1KS217A06A37 : with start stop, emergency stop, padlocking.

Schneider Electric UK