{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What size cables can be terminated into NSX400-630 MCCBs when fitted inside an NS MCCB feeder pillar.
Compact NSX MCCB types NSX630 / NSX400 will accept cables up to 185mm with standard width cable lugs.
If terminating 240 or 300mm cables, then the 52mm cable spreaders or the special MG reduced width cable lugs should be used.
This is based on a single core Cu cables.

Schneider Electric UK