{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can I remotely reset the LT47 electronic overload relay
The LT47 Electronic Overload is available in two formats

LT47***S - With Manual or Electric Reset
LT47***A - with Automatic Reset

Electric reset is only available in the LT47***S
To perform an Electric Reset : Interrupting control power (minimum 0.1s).

wiring diagram

Schneider Electric UK

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.