{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can the class 20 LRD15** thermal overloads be used with LC1D38** contactors?
Yes, although the LRD15** overload setting range only goes up to 32 amps you can fit any one of these overloads to an LC1D38** contactor.

The LC1D38** contactor shares the same frame body as the LC1D25** and the LC1D32** contactors.

Note: There are alternatives in the new range, which allow setting ranges to cover most of the Tesys D range. See the attached catalogue extract for further information.

** = Coil voltage code in the case of contactors, and digits representing current setting range in the case of thermal overloads

Schneider Electric UK

Attachment(s)
LRD Class 20.pdf [827.81 KB]