{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Are security screws essential for use with Clipsal E Series products?

The E Series product range is made from impact resistant polycarbonate and is suitable for use in a variety of environments and applications.  Whilst they are not essential, the use of security screws (product code 31J) is recommended where additional peace of mind is required. 31J security screws are designed to be installed on the reverse of all E Series switches. The addition of 2 x security screws per switch prevent the switch mechanism from being dislodged after installation.

Schneider Electric UK

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: