{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What information is required to correctly select (specify) a contactor?

Although the contactor is probably one of the most common components in an industrial / motor control application, selecting one correctly requires detailed application information to be provided.

There are 3 key elements to a contactor;
  • Main contacts (also referred to as main poles)
  • Auxiliary contacts
  • Coil (part of the electromagnet used to energise the contactor).
Each of these elements should be fully specified based on the application;

1. Main pole selection criteria;

  • How many required in either normally open (N/O) or normally closed (N/C) format
  • Current rating in amps.
  • Voltage rating in AC or DC
  • Duty (either AC1, AC3, DC1- DC5 etc). In the absence of a specific duty, a full description of the nature of the electrical load (e.g. lighting , resistive heating etc), making current, breaking current and continuous current through the contacts.
2. Auxiliary contacts selection criteria;
  • How many required in either normally open (N/O) or normally closed (N/C) format. Possibility of time delayed auxiliary contacts with certain product ranges.
  • If not used in standard low power signalling application, details as per main poles required.
3. Coil selection criteria;
  • Voltage of coil (Note: The coil is often a different voltage to the main poles).
  • AC or DC voltage;
    • Frequency of coil if AC.
    • If DC coil, is low consumption required (available for certain ratings of TeSys D and TeSys K contactors).
Any additional information available should be provided, such as;
  • Is the contactor to be enclosed, i.e. is an enclosed motor starter required?
  • Specific design requirements (e.g. Modular)
  • Number of operations per hour
  • latching operation
  • Environmental considerations such as ambient temperature etc.
  • Are any ancillary parts required such as mechanical interlocks, busbars, thermal overload relays or motor protection circuit breakers?







Schneider Electric UK

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.