undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the AC3 rating of the LC1DT60A and LC1DT80A 'Everlink' TeSys D contactors?
The 4 pole versions of the 'Everlink' TeSys D contactors are designed for AC1 applications. 

Although theoretically unnecessary*, occasionally a request for a 4 pole AC3 rated contactor will be made. Due to the very small number of applications that genuinely require 4 poles and an AC3 level of performance, this capability has not been included in the specification of the LC1DT60A.. and LC1DT80A.. 'Everlink' TeSys D contactors.

In the event that an AC3 level of performance is required between 40A and 80A, the LC1D80004.. (part number to be completed according to coil voltage#) could be considered. This contactor has 4 poles and has an AC3 rating of 80A (refer to catalogue for full performance figures).


*AC3 is the utilisation category for starting 3 phase squirrel cage induction motors and consequently only 3 poles are normally necessary.
#  For coil voltage codes see FAQ number; FA135911.
 

Schneider Electric UK

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
move-arrow-top
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.