{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What Schneider Electric Drive has replaced the Telemecanique Altivar 11 (ATV11)?

The replacement Drives for the ATV11's are the ATV12's

The chart below shows the nearest equivalents:

Single phase 110 volts input to three phase 220 output
ATV11HU05F1AATV12H018F1
ATV11HU09F1AATV12H037F1
ATV11HU18F1AATV12H075F1

Single phase 200-240 input to three phase 200-240 output standard heat sink version drive
ATV11HU05M2EATV12H018M2
ATV11HU09M2EATV12H037M2
ATV11HU12M2EATV12H055M2
ATV11HU18M2EATV12H075M2
ATV11HU29M2EATV12HU15M2
ATV11HU41M2EATV12HU22M2

Three phase 200-240 input to three phase 200-240 output standard heat sink version drive
ATV11HU05M3AATV12H018M3
ATV11HU09M3AATV12H037M3
ATV11HU18M3AATV12H075M3
ATV11HU29M3AATV12HU15M3
ATV11HU41M3AATV12HU22M3

Single phase 200-240 input to three phase 200 -240 output plate version drive
ATV11PU09M2EATV12P037M2
ATV11PU12M2EATV12P055M2
ATV11PU18M2EATV12P075M2

Note: Please be aware that there are differences between the ATV11 and ATV12, please refer to documentation to establish that the new product meets your technical requirements

Schneider Electric UK