{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the minimum and maximum thickness of wall our dry lining boxes (GDL1 & GDL2) can be installed in?
The minimum thickness is 2 mm and the maximum thickness is up to 17 mm.

Schneider Electric UK

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: