{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the resistance of our XB4 and XB5 heads to salt spray?

Article available in these languages: French

The anti-corrosion performance of surface-treated XB4 and XB5 metal and plastic bezel heads are verified by testing in accordance with ISO 9227, NF 41-002, DIN 50021 and ASTM B117. These standards describe the salt spray test, which involves spraying a solution of water and salt (NaCl) onto the components until the first signs of corrosion (white rust) appear or red rust appears.

The results are as follows:

  • XB4, metal bezel head (nickel surface treatment) => resistance B2 (superficial attack)
  • XB5, plastic bezel head => resistance B5 (slight discoloration). Initial TH treatment - IP65 and IP66 protection with addition of transparent boots: ZBPA/ZBP0/ZBP0A.

For key heads protected by a zinc-nickel electroplated coating, salt spray tests performed in accordance with IEC 68-2-11 show the appearance of a deposit of white rust after 160 hrs and the appearance of a deposit of red rust after 1500 hrs.

Schneider Electric UK