The PLC programming cable via PC USB port, part number TSXPCX3030, is replaced by TSXCUSB485. This is a multifunction programming cable which can be used for multiple types of hardware connection and configuration, consequently the use of a second cable (link cable) is required; please consult the diagram below:
The reference provided as alternative in this FAQ (TSXCUSB485) was discontinued on 20 October 2023.
Consider the migration of the device you are trying to use for a new technology.