In order to program the XBT Magelis we need to use the XBT-L1000 software.
To have more than 16 alarms, the number of words associated with the alarms must be changed in the dialogue table in order to have the n x 16 alarms required as it is shown below:
To have more than 16 alarms, the number of words associated with the alarms must be changed in the dialogue table in order to have the n x 16 alarms required as it is shown below:
Note: The Magelis range is now Harmony. Please get access to our digital catalog https://digicat.se.com/ or contact our support center for more information about migrations to a newer platform. |