{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between a single-turn and a multi-turn encoder?
Single turn encoder

This type of encoder does not store information on the "number of turns". For each position of the shaft, it delivers a single data item in the form of a "word" in parallel or serial mode, which can be read directly and quickly by control systems.
 
Multiturn encoder

This type of encoder can perform a greater number of turns and delivers, in addition to the position of the shaft in the turn, the number of turns performed in relation to a reference point.

Schneider Electric UK

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
move-arrow-top