{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
When is the Isobar neutral link used?
Neutral links are used to link between the neutral incomer and the neutral of the outgoing device
When: 1P&N outgoing breaker is used in Isobar type A board or B board.
4 pole outgoing breaker is used in Isobar type B board.

Schneider Electric UK

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: