{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Do I need 2 Tesys U bases (LUB12, LUB32, LUB38) for reversing operation?

The answer is no. There are multiple ways of creating a reversing starter, depending on the base module you choose. Some are built into the starter and others are add-on, but in all cases you only need one Tesys U base module.

There are 3 possible ratings for the base; 12A, 32A and 38A. Each are available in two configurations; Standard and Advanced. This depends on whether you want to use communications / advanced protection modules. Options can be found in the catalogue section, chapter A4.

You can download it here:

  1. Go to www.se.com
  2. In the search bar at the top type in A4 Tesys
  3. Click on the result under "documents" that says "Tesys - Chapter A4..."
  4. Click Download

Schneider Electric UK