{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the maximum distance between the current transformer and the meter?
The maximum distance depends on the equipment you are using. the chosen CT must be able to supply enough power (VA) and still maintain the accuracy level (Class).

Attached file, helps choose the smallest size CT according to your choosen meter, CT and cable length. Please note that the cable length on this file is one way only (S1), the distance between CT and meter without the way back (S2).

The part number of the CT provided by the file must be checked against the mechanical sizes of cables/bars.

Schneider Electric UK

Attachment(s)
CT Calc tool V1.2.xlsx [31.17 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: