{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
NSX Single pole terminal shield LV429320 is in the catalogue but not on the system?
Unfortunately there is an error in the Ready to Install catalogue SE8863 JAN 2015 on page 8/18.

The part number LV429320 is incorrect

The correct part number should be LV438320 (Pair of single pole terminal shields)

Schneider Electric UK

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.