{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Are the NSX 250,160 & 100 the same size?
Yes, the frame size of the NSX 250A , 160A & 100A is the same size dimensionally, providing the number of poles is the same.

And the Dimentions W X H X D for a 2/3P  are 105 X 161 X 86 mm and for 4P are 140 X 161 X 86 mm.

Schneider Electric UK

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.