{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between the NSX250F and NSX250N?
This applies to the 100 and 160Amp frame size also.
Compact NSX - NSX250F

The only difference is the Icu kA fault breaking capacity @ 380/415 AC
NSX250F = 36 kA,
NSX250N = 50 kA
NSX250H = 70 kA
NSX250S = 100 kA
NSX250L = 150 kA
Otherwise the MCCB's have the same fit and function.

Schneider Electric UK

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.