{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How do the different versions of MTZ breakers connect to Ethernet?
We provide the following ways to connect MTZ to Ethernet:

For withdrawable MTZ (most probably Playbook3), 2 ways are possible:
  • 1) Use ULP port (standard) + EIFE (Embedded IFE, optional), providing an immediate ready-to-use Ethernet connection.
  • 2) Use ULP port (standard) + IFE or IFE gateway (optional)
For fixed MTZ (most probably Playbook1), you can use the ULP port (optional) + IFE or IFE gateway (optional).

See Attachment:

Schneider Electric UK

Attachment(s)
Capture.PNG.png [258.23 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.