{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the function codes of the Modbus protocol used by IO Scanning in TCP-IP for a M241/M251 controller?
The following Modbus protocol function codes are used by IO Scanning on Modbus TCP-IP over Ethernet :
  • Read only   = function code 03
  • Write only   = function code 16
  • Read/write  = function code 23

Schneider Electric UK