{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Why does the Sepam Series 20, 40 and 80 Relay not display waveforms for all phases of current/voltage?
When certain variables are calculated rather than acquired (measured) by Sepam, the waveform associated to those variables is not available. Those variables are calculated by a software program, based on the "phasors" derived from signal processing ("sin/cos" filter). For those variables, "not valid" appears in the related field in the disturbance recording file. This may occur for I2, Ir, Vr, U32, U13, according to the set-up. See the example below.
Calculated variables

Schneider Electric UK