{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How do you add a image or picture in EcoStruxure Operator Terminal Expert (former Vijeo XD)?
To add an image in to the project you have to drag in the "Image" icon from the Tool Chest and the allocate an image file in the properties for the icon.
Please watch the video below which shows the process (The video is done in Vijeo XD):


Note in Vijeo Designer the function is different, the addition of a picture is added in the using the "Image" function in the "Toolbar"

We have the possibility to add images into the library object of EcoStruxure Operator Terminal Expert as i show in the next video:

https://youtu.be/PzG_TUzpYRo

This will allow to see the images in the project library BUT those images will not be linked to the project only to your PC, so if you share the project or open it in another laptop the images used in the project will not be seen. If you want to avoid that then you will need to add each image in to the project using the object for images.

Schneider Electric UK