{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to programme / setup a Wireless pushbutton in the Harmony XB5R or XB4R range?
Please watch the video which shows how to program a single contact on the base unit with a push button.

IFrame video

The Harmony XB5 and XB4 ranges are very adaptable and there are multiple functions available using a single pushbutton.

Attached below is a quick programming guide which shows many of the other possible functions and how to achieve them. You can also find further detail in the instruction sheets provided on our website, here:
  1. Go to www.se.com
  2. Type the part number of your relay unit into the search bar (for example ZBRRA used in this video)
  3. Click on the result under "In Product Datasheets"
  4. Download instructions in the "documents" tab
The products used in the video are :
  • ZBRRA Configurable Receiver (with Output Functions: Monostable, Bistable, Start / Stop)
  • ZB5RTA4 Red Flush Push button (Plastic)
  • ZBRM22 Plastic Enclosure (2 cut outs)
NOTE that the ZB5RTA pushbuttons are no longer used, as we have released a new transmitter which is compatible with the standard XB4/XB5 range of pushbuttons. Please refer to the catalogue for more information. This can be found at digicat.se.com, our online database of industrial catalogues.

Schneider Electric UK

Attachment(s)
XB5 Wireless Pushbutton - Quick Programming Guide.pdf [211.66 KB]