Search FAQs
Can I use Canalis in DC?
There is no problem with using the Canalis KTA, KTC & KH trunking in DC.
Determination of direct current that can be conveyed:
The power conveyed in a busbar trunking is limited by the maximum permissible temperature rise.
In standard AC three-phase conditions, distribution is considered to be balanced and the current in the neutral is thus estimated equal to zero. Power loss in heat form = Pac= 3x R x Iac²
(R= resistance of a conductor, Iac = rms current in conductor)
In DC conditions, if we consider 1 conductor for the + and 1 conductor for the -, power loss for 4 conductors = Pdc = 4 x R x Idc² (Idc = direct current) Total power loss in heat form must remain constant: Pac = Pdc
- Case with 1 conductor for the + and 1 conductor for the ? (2 possible circuits in the same busbar trunking) Idc=1,7320/2 xIac=0.866xIac
- Case with 2 parallel conductors for the + and 2 parallel conductors for the - (1 circuit in the same busbar trunking) Idc=1,732xIac
If the DC short-circuit peak current is equivalent to or greater than the standard short-circuit peak current, interlacing is necessary
If the DC short-circuit peak current is less than the standard peak short-circuit current, contact us to evaluate the electrodynamic forces generated
- Case with 1 conductor for the + and 1 conductor for the - (2 circuits available in one busway)
- Case with 2 parallel conductors for the + and 2 parallel conductors for the ? (1 circuit available in one busway)
Reduced electrical equation: U network = R x Isc + Uarc Isc
=> (U network -Uarc) / R = Isc
Isc = 0 when Uarc = U network
Rapid increase in arc voltage is possible by the placing in series of fuse protection devices: one fuse on the + and one fuse on the - of each circuit.
For certain operational current and fuse characteristics, it may be necessary to implement two fuses connected in series by polarity (highly inductive circuit). In some cases, two fuses must be connected in parallel by polarity. According to applications, the standard enclosures supplied with only three fuse bases cannot therefore always be used
Determination of direct current that can be conveyed:
The power conveyed in a busbar trunking is limited by the maximum permissible temperature rise.
In standard AC three-phase conditions, distribution is considered to be balanced and the current in the neutral is thus estimated equal to zero. Power loss in heat form = Pac= 3x R x Iac²
(R= resistance of a conductor, Iac = rms current in conductor)
In DC conditions, if we consider 1 conductor for the + and 1 conductor for the -, power loss for 4 conductors = Pdc = 4 x R x Idc² (Idc = direct current) Total power loss in heat form must remain constant: Pac = Pdc
- Case with 1 conductor for the + and 1 conductor for the ? (2 possible circuits in the same busbar trunking) Idc=1,7320/2 xIac=0.866xIac
- Case with 2 parallel conductors for the + and 2 parallel conductors for the - (1 circuit in the same busbar trunking) Idc=1,732xIac
- Electrodynamic effect:
If the DC short-circuit peak current is equivalent to or greater than the standard short-circuit peak current, interlacing is necessary
If the DC short-circuit peak current is less than the standard peak short-circuit current, contact us to evaluate the electrodynamic forces generated
- Voltage drops :
- Case with 1 conductor for the + and 1 conductor for the - (2 circuits available in one busway)
- Case with 2 parallel conductors for the + and 2 parallel conductors for the ? (1 circuit available in one busway)
- Protection:
Reduced electrical equation: U network = R x Isc + Uarc Isc
=> (U network -Uarc) / R = Isc
Isc = 0 when Uarc = U network
Rapid increase in arc voltage is possible by the placing in series of fuse protection devices: one fuse on the + and one fuse on the - of each circuit.
For certain operational current and fuse characteristics, it may be necessary to implement two fuses connected in series by polarity (highly inductive circuit). In some cases, two fuses must be connected in parallel by polarity. According to applications, the standard enclosures supplied with only three fuse bases cannot therefore always be used
Released for:Schneider Electric UK
Explore more
Range:
Explore more
Range: