{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can a standard inductive sensor be used to detect stainless steel, brass, aluminum, copper, lead or bronze?
Yes, however, a correction coefficient will have to be applied to the sensing range.
Please check attached catalogue print screen for the different values.

The exception to this rule is our Factor 1 (Fe/Nfe) range. On this particular range, the sensing range is the same regardless the material to be detected.

Schneider Electric UK

Attachment(s)
Km.png [222.95 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.