{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to fit Arc Fault Device (Acti9 Active) on the dinrail enclosure with the AFDD comb Busbar?
Acti9 Active AFDD to install on a DIN Rail an extension enclosure with a DIN rail is required for installation (retrofit or new one).

The extension enclosure can be placed below or a side of main enclosure. You can refer to the extension enclosures section listed into the Acti9 Isobar P catalogue.

In case you intent to use the "all in one" Acti9 Active product, you should consider 2 no.s of terminal block (SEA9TB1001) as an incomer (Phase & Neutral) to the AFDDs for 1 phase supply & 4P of terminal blocks (SEA9PTB1254) for 3 phase supply or appropriate switch disconnector based on the supply
Needs:
  1. Extension enclosure with DIN rail (ex SEA9BNEX034N or SEA9BN8SXS)
  2. Terminals blocks (SEA9TB1001) / Isolator Switch to supply phase & neutral to Acti9 Active product
  3. Acti9 Active devices
    Number of possible AFDD's that can be fitted
    SI. NoCRDescriptionNo. of AFDD's
    1SEA9XPH114A9 Comb busbar 1P+N, 100A, 14 O/G Mod7
    2SEA9XPH312A9 Comb busbar 3P+N, 100A, 12 O/G Mod6

Schneider Electric UK