{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Migration - Is it possible to migrate an XBTL-1000 application to Vijeo Designer?
It is possible to migrate an application made in XBT-L1000 (discontinued) to Vijeo Designer by using the software called "Switch2Vijeo" but there are some considerations in order to use this software:

•Vijeo Designer must be V5.1 SP2
•XBT-L1000 must be V4.51
•File Extension must be *.dop

Once we have the application in Vijeo Designer v5.1 SP2 we can use any higher version of Vijeo Designer.

Note 1: It is possible that some manual modification need to be done to adjust your new application.
Note 2: Use a virtual machine to install those software ( Windows XP)

Schneider Electric UK

Attachment(s)
Switch2Vijeo.zip [34.68 MB]
XBTL1000_V4.51.zip [384.27 MB]
Migration - Is it possible to migrate an XBTL-1000 application to Vijeo Designer?
It is possible to migrate an application made in XBT-L1000 (discontinued) to Vijeo Designer by using the software called "Switch2Vijeo" but there are some considerations in order to use this software:

•Vijeo Designer must be V5.1 SP2
•XBT-L1000 must be V4.51
•File Extension must be *.dop

Once we have the application in Vijeo Designer v5.1 SP2 we can use any higher version of Vijeo Designer.

Note 1: It is possible that some manual modification need to be done to adjust your new application.
Note 2: Use a virtual machine to install those software ( Windows XP)
 

Schneider Electric UK

Attachment(s)
Switch2Vijeo.zip [34.68 MB]
XBTL1000_V4.51.zip [384.27 MB]
Explore more
Product:
Range:
Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
Explore more
Product:
Range:
move-arrow-top