{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the high temperature HL100 and HL300 limit switches the same size as the standard L100 and L300 equivalent?
Issue:
Is there a difference in the size of the HL100/HL300 and the L100/L300?

Product Line:
R.B. Denison Lox-Switch

Environment:
Limit Switches

Resolution:
Yes, the L and HL switches are the same dimensionally.

Schneider Electric USA