{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is a stainless steel NEMA 4X enclosure available in the NQ panel?
Issue:
Does Square D offer a NEMA 4/4X stainless steel enclosure for the NQ interiors?

Product Line:
Lighting and distribution panelboards

Environment:
NQ panelboards sold in the United States.

Cause:
Product availability.

Resolution:
Yes, only as a factory assembled panel.  It should be entered as Type 4/4X stainless steel in the product selector.

Schneider Electric USA