Issue:
Product design features
Product Line:
HD Safety Switch
Cause:
Terminal lug data
Resolution:
ALL the 1200amp Heavy Duty Safety Switches will accept (4) #3/0 AWG - 750 kcmil aluminum or copper conductors per phase. The Lug conductor(or wire) temperature rating is 75 degree C.
The only alternate lugs are the H12LKE2 compression lug kit, but the compression lugs do NOT allow for any additional or larger wires. See FA120694 for more information on this compression lug kit.
More information on Safety Switches here.
Product design features
Product Line:
HD Safety Switch
Cause:
Terminal lug data
Resolution:
ALL the 1200amp Heavy Duty Safety Switches will accept (4) #3/0 AWG - 750 kcmil aluminum or copper conductors per phase. The Lug conductor(or wire) temperature rating is 75 degree C.
The only alternate lugs are the H12LKE2 compression lug kit, but the compression lugs do NOT allow for any additional or larger wires. See FA120694 for more information on this compression lug kit.
More information on Safety Switches here.