{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the Terminal Lug Data for ALL of the 400amp, US and Canada, Heavy Duty Safety Switches (For example, HU365RB,CH225N, CH225NAWK, H365, H365AWK, H365DS and CH3665DS)?

Issue:

Product Design Features

Product Line:
Heavy Duty Safety Switch

Cause:
Terminal lug data

Resolution:

The 400amp Heavy Duty Safety Switches will accept (1) 1/0 AWG - 750 kcmil Al/Cu OR (2) 1/0-300kcmil Al/Cu conductors per phase. The Lug conductor(or wire) temperature rating is 75 degree C.
With the exception of the following;
Maximum wire bending space for the Type 4/4X/5 Stainless Steel and Type 12 Switches will allow for (1) 600kmcil Al/Cu or (2) 300kcmil Al/Cu conductors per phase.

NOTE: The only alternate lugs are compression lugs and they do NOT allow for any different wire size or quantity than what is shown above.



Schneider Electric USA