Search FAQs
Can subfeed lugs be added to Homeline load centers?
Issue:
Are field installable subfeed lug kits available for Homeline Load centers?
Product Line:
Homeline
Resolution:
Yes. For subfeed lug applications up to 125 ampere maximum, use HOML2125. Do not exceed the load center mains ampacity rating.
For subfeed lug applications up to 225 ampere, use HOML2225. The HOML2225 can be applied only in a Square D Homeline convertible mains, single phase load center, Series S01 or later, RATED 150 AMPERE OR GREATER. Do not exceed the load center mains ampacity rating.
NOTE: DO NOT USE in other manufacturers load centers or panelboards. Please refer to the Installation Bulletin supplied with the device for further restrictions regarding mounting this device or adjacent branch circuit breakers.
Are field installable subfeed lug kits available for Homeline Load centers?
Product Line:
Homeline
Resolution:
Yes. For subfeed lug applications up to 125 ampere maximum, use HOML2125. Do not exceed the load center mains ampacity rating.
For subfeed lug applications up to 225 ampere, use HOML2225. The HOML2225 can be applied only in a Square D Homeline convertible mains, single phase load center, Series S01 or later, RATED 150 AMPERE OR GREATER. Do not exceed the load center mains ampacity rating.
NOTE: DO NOT USE in other manufacturers load centers or panelboards. Please refer to the Installation Bulletin supplied with the device for further restrictions regarding mounting this device or adjacent branch circuit breakers.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: