undefined [object Object]
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the QOM22225NF, QOM22225NS and QOM22225NRB circuit breaker enclosures suitable for use as service entrance equipment?
Issue:
Product Design Features

Product Line:
QOM2 Circuit breaker enclosures

Environment;
Service Entrance Rating

Cause:
application

Resolution:
These enclosures are NOT Service Entrance Rated where the new code is being enforced requiring the Service Entrance Barriers. Square D does not offer any Service Entrance Barriers for the QOM2 Enclosures. Consider using the Q-Frame Enclosures. SEE CURRENT ON-LINE DIGEST For Catalog Numbers.

These enclosures are "Suitable For use as Service Equipment" and Marked that way, but ONLY in the locations where the most current code has not yet been adopted that requires the Service Barriers. 
 

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
move-arrow-top