{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What does the 24 Vdc power supply do when provided on an ammeter trip unit for P-frame, R-frame, and Masterpact breakers?
Issue:
What does the 24 Vdc power supply do when provided on an Ammeter trip unit for P-frame, R-frame, and Masterpact breakers?

Product Line:
Powerpact P-frame, Powerpact R-frame, Masterpact

Resolution:
Without the 24V DC power supply the Ammeter trip unit:
  • Provides fault protection for LSIG functions
  • Provides LED trip indication (powered by an onboard battery)
  • Ammeter and bar graph powers with the current flow on one phase of 25% or more of the sensor rating.
  • Ground fault push-to-trip button works for testing ground fault with current flow on one phase of 25% of the sensor rating or more.

With the 24V DC power supply wired to F1 (- terminal) and F2 (+ terminal) on the terminal block on top the the trip unit, the Ammeter trip unit:
  • Provides all of the above
  • Ammeter and bar graph displays are functional below 20% of the sensor rating current flow on one phase
  • Ground fault push-to-trip button works for testing ground fault with no current flowing through the breaker
  • Highest fault current reading and phase that tripped
  • Optional Modbus communications

Ground fault push-to-trip button will also be functional if a hand held test kit or full function test kit is powering the trip unit.

Schneider Electric USA