Issue:
What are the repair part components to the 80110-TFL-50?
Product Line:
NQOD Panelboards
Environment:
NA
Cause:
Repair parts
Resolution:
The installation of this kit allows an NQOD42L225TFL, NQOD42L225CUTF, NQOD442L225TFL or NQOD442L225CUTF interior to be installed in an MH47 (MLO) or MH62 (M/B). It includes:
(1) 80110-067-03 Left TFL mtg rail
(1) 80110-067-04 Right TFL mtg rail
(2) 80110-007-05 D/F mtg brackets
(10) 80025-067-01 Screws
(4) 21590-17081 Rail extension screws
(2) 29215-52126 Rachet fasteners
(1) 80110-045-01 TFL deadfront
(1) 80110-071-02 Branch deadfront
What are the repair part components to the 80110-TFL-50?
Product Line:
NQOD Panelboards
Environment:
NA
Cause:
Repair parts
Resolution:
The installation of this kit allows an NQOD42L225TFL, NQOD42L225CUTF, NQOD442L225TFL or NQOD442L225CUTF interior to be installed in an MH47 (MLO) or MH62 (M/B). It includes:
(1) 80110-067-03 Left TFL mtg rail
(1) 80110-067-04 Right TFL mtg rail
(2) 80110-007-05 D/F mtg brackets
(10) 80025-067-01 Screws
(4) 21590-17081 Rail extension screws
(2) 29215-52126 Rachet fasteners
(1) 80110-045-01 TFL deadfront
(1) 80110-071-02 Branch deadfront