{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for a CM200S, Series M01?
Issue:
Repair parts list for CM200S, series M1

Product Line:
CSEDs

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4053414150
Main Breaker Section Cover Assembly - 4053449250
Main Breaker Section Cover Hinges - (2) X2983
Main Breaker Section Cover Hinge Mounting Screws - (2) 2159414081
Dead Front Interior Trim - 4053443601 (also requires insulator and rivets, below)
Dead Front Interior Trim Insulator - 4053435601 (attaches to rear of interior trim)
Dead Front Interior Trim Insulator Rivets - (2) 2430313230
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws, but only one screw is required to secure the trim)
Meter Base Assembly - 4053448450 (includes meter base, (2) line side lugs, (4) meter jaws, (4) meter jaw blade guides, and load side bussing)
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Nuts - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Left Line Side Lug Assembly - 4053408750
Right Line Side Lug Assembly - 4053408850
Meter Sealing Ring - 2920910001
Closing Cap - (2) ACP
Main Breaker - QOM2-VH type, 200A maximum
Main Breaker Mounting Nuts - (2) 2342702001
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: