{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for a PAK75PG, Series E03 ServicePak power outlet panel?
Issue:
Design Repair parts

Product Line:
Power Outlet Panels

Resolution:
Only the parts listed below are considered field replaceable.
Panel Cover - 4054025101
Panel Cover Mounting Screw - (2) 2142717161
Pedestal Cover - 4054013801
Pedestal Cover Mounting Screw - (2) 4020513001K
Vapor Barrier Kit - 4028312851
Interior Trim - 4054024702
Interior Trim Mounting Screw - (2) 4020513001K
Interior Assembly - 4054020251 (base assembly not included)
Base Assembly - 4054008650
Circuit Breaker - QO120GFI, QO130, and QO250
Receptacle - 4054001450 (125 volt/20 amp), 4054004450 (125 volt/30 amp), and 4054027950 (125/250 volt/50 amp)
Receptacle Mounting Screw - 2190312160 (2 required for the 125 volt/20 amp receptacle)
Receptacle Mounting Spring Clip - 2330100001 (2 required for the 125 volt/20 amp receptacle)
Receptacle Mounting Screw - 2159412120 (3 required for the 125 volt/30 amp receptacle; 2 required for the 125/250 volt/50 amp receptacle)
Loop Feed Phase/Neutral Lugs Assembly - 4054014551
Loop Feed Lugs Assembly Mounting Screw - (4) 2159417121
Loop Feed Ground Lug - (2) 4025104251
Loop Feed Ground Lug Mounting Screw - (2) 4020600903
Ground Bar - 4023089855
Ground Bar Mounting Screw - 4020547901
NOTE: Covers and Interior Trims do not have labels applied.

Schneider Electric USA