Search FAQs
Are Square D/Schneider Electric's 9070 Type T or TF Control Transformers varnish dipped and baked, Vacuum Pressure Impregnated (VPI), or Epoxy Encapsulated?
Issue:
Specifications may call for Vacuum Pressure Impregnated (VPI) Control Transformers
Product Line:
LV Transformers
Environment:
Applies to Class 9070 Type T and TF Control Transformers
Cause:
Vacuum Pressure Impregnated (VPI) Control Transformers have greater resistance to corrosion and other damage to the core and copper windings
Resolution:
Square D's 9070 Type T and TF Industrial Control Transformers, the premier product in the industry, are Vacuum Pressure Impregnated (VPI) with a polyester varnish, then baked to seal out moisture and other contaminants.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: