{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the replacement lugs for EDB, EGB, EJB, FDA, FGA, and FJA breakers?
Issue:
What are the replacement lugs for EDB, EGB, EJB, FDA, FGA, and FJA breakers?

Product Line:
I-Line Panels, NF Panels, FA frame breakers, E-Frame Breakers

Resolution:
 Cat # Amp Wire Range Instruction Bulletin
 AL30FD 15-30 A one #12—#6 AWG Al or one #14—#6 AWG Cu48840-098-02
 AL100FD 35-125 A one #12—2/0 AWG Al or one #14—2/0 AWG Cu
 CU100FD 15-125 A one #14—1/0 AWG Cu

Notes
  • In the standard 15-30 A EDB, EGB, and EJB breakers, high amp lugs can be factory installed with suffix LH. If they are not ordered factory installed, standard high amp lug kit AL100FD CANNOT be used on the 15-30 A breakers. Copper high amp lug kit CU100FD can still be used even if the breaker was not ordered with high amp lugs.
  • Each lug kit contains (3) lugs.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top