Search FAQs
Can the SDSA1175 or SDSA3650 be used outdoors?
Issue:
Application of SDSA1175 or SDSA3650 on outdoors.
Product Line:
Surge Protection.
Environment:
Products sold in the United States.
Cause:
Product features.
Resolution:
Yes, these devices are suitable for indoor (NEMA 1) or outdoors (NEMA 3R) applications.
CTA-ID : 2007158
Application of SDSA1175 or SDSA3650 on outdoors.
Product Line:
Surge Protection.
Environment:
Products sold in the United States.
Cause:
Product features.
Resolution:
Yes, these devices are suitable for indoor (NEMA 1) or outdoors (NEMA 3R) applications.
CTA-ID : 2007158
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: