{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the H362DS, series F6? (may be shown as F06)
Issue:
What are the repair parts for the H362DS, series F6? (may be shown as F06)

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the H362DS, series F6 (F06) are as follows. No other parts are available.
Line Base Assembly - 4056603850 (arc suppressor not included)
Load Base Assembly - 4056604050
Line & Load Base mounting screw - 4020515101 (3 for line and 2 for load)
Arc Suppressor Assembly - HAS0610F (includes arc suppressor, mounting screw, and instructions)
Lug Assembly - 4025101652 (per lug, line and load)
Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
Handle Coupling - 4056699850
Cover Interlock Defeat Coupling - 4056699750
Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
Lockplate mounting screw - 2194918121 (2 required)
Ground Lug - 4025101652 (2 required)
Ground Lug Mounting Screw - 4020513503
Fuse Pullers - FPK0610 (1 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: