undefined [object Object]
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a convertible, main lug, QO load center be used on a 240 Vac, grounded B phase delta system if the main lugs are converted to a main breaker?
Issue:
Product Design feature

Product Line:
QO load centers

Resolution:
No, if the main lug load center is converted to a main breaker load center, it cannot be used on the 240 Vac, grounded B phase delta system. The QOM1-VH and QOM2-VH main breakers are not UL Listed for use on this voltage system.

Schneider Electric USA

Can a convertible, main lug, QO load center be used on a 240 Vac, grounded B phase delta system if the main lugs are converted to a main breaker?
Issue:
Product Design feature

Product Line:
QO load centers

Resolution:
No, if the main lug load center is converted to a main breaker load center, it cannot be used on the 240 Vac, grounded B phase delta system. The QOM1-VH and QOM2-VH main breakers are not UL Listed for use on this voltage system.

Schneider Electric USA
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
Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top