{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the torque rating for the DZ2F** lugs?
Issue:
Need to know the torque rating for the DZ2F** lugs

Product Line:
Contactors and Starters - IEC

Environment:
TeSys™ F Contactors

Resolution:
Based on specific lug used per the following:

Bolt Lug To Contactor
DZ2FF1 & DZ2FF6 = 89 lb. - in.
DZ2FG1 & DZ2FG6 = 160 lb. in.
DZ2FH1 & DZ2FH6 = 310 lb. - in.
DZ2FJ1 & DZ2FJ6 = 310 lb. - in.
DZ2FK1 & DZ2FK6 = 310 lb. in
DZ2FL1 & DZ2FL6 = 510 lb. - in.
DZ2FX1 & DZ2FX6 = 510 lb. - in.

Wire Pressure Screw
DZ2FF1 & DZ2FF6 = 120 lb. - in.
DZ2FG1 & DZ2FG6 = 200 lb. in.
DZ2FH1 & DZ2FH6 = 275 lb. - in.
DZ2FJ1 & DZ2FJ6 = 500 lb. - in.
DZ2FK1 & DZ2FK6 = 500 lb. in
DZ2FL1 & DZ2FL6 = 500 lb. - in.
DZ2FX1 & DZ2FX6 = 500 lb. - in.

Schneider Electric USA