{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a QBL, QDL, QGL, or QJL circuit breaker be used to replace a Q2L, Q2L-H, or Q2LH circuit breaker in an individually mounted Q2 enclosure?

Article available in these languages: Spanish

Issue:
Breaker replacement

Product Line:
Q Frame breaker enclosures

Resolution:
Yes, the Q2 enclosures, Q22200NS, Q22200NRB, Q23225NF, Q23225NS, and Q23225NRB, will accept the PowerPacT Q frame circuit breakers. However, restrictions regarding the short circuit rating may apply. The enclosures marked for use with the QBL, QDL, QGL, or QJL breakers are designated series E05. For retrofitting these breakers into existing series E03 or earlier enclosures, restrictions regarding short circuit current ratings apply.

The following statements are on the wiring diagrams of the series E01 and E03 enclosures: "The short circuit rating of this enclosure is equal to the interrupting rating at the supply voltage marked on the circuit breaker installed, but not to exceed 42,000 RMS Symmetrical Amperes at 240Vac." and "Replacement circuit breakers must have an interrupting rating equal to or greater than that of the circuit breaker originally installed".

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
move-arrow-top