{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How many pole spaces are required to mount a QO60SL , QO2125SL, or QO3125SL into a QO load center?
Issue:
Product Design Features

Product Line:
Homeline and QO load centers

Resolution:
The QO60SL and QO2125SL require two pole spaces. The QO3125SL is only for three phase QO load center applications and requires three pole spaces.

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: