{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Should an antioxidant be used on the QO or Homeline load center main lugs?
Issue:
Application

Product Line:
Load Center

Resolution:
The use of an antioxidant on the load centers main lugs is not required. The lugs are UL listed for use with copper or aluminum conductors without the use of any antioxidation supplement. The use of an antioxidant is not prohibited, but assure that the brand used is a NON-PETROLEUM based product. If a petroleum based product is used, and comes in contact with the insulating base, it can degrade the insulating base material.

Schneider Electric USA