{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the recommendations regarding conduit sizing and type of wire for the installation of a Hospital Isolated Power System?
Issue:
Recommendations regarding conduit sizing and type of wire for the installation of a Hospital Isolated Power System.

Product Line:
Medical Products

Environment:
Installation

Cause:
Recommendation

Resolution:
Square D recommends a minimum conduit diameter of 3/4``, one circuit per conduit, a maximum of 360 degrees of bend per conduit run, and absolutely no pulling compound of any type. The recommended wire is XHHW-2. Additional references are NFPA 99 and NEC Article 517.


Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: