{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What UL Standards and file numbers are double throw safety switches tested and listed under?
Issue:
Testing and Listing

Product Line:
Double Throw Safety Switches

Resolution:
The double throw safety switches are tested to UL98, "Standard for Safety - Enclosed and Dead-Front Switches". Additional UL standards may be referenced within UL 98 for compliance to that standard. The double throw safety switches are listed in UL File E2875. 
NOTE: There are a very few of the double throw catalog numbers that are NOT UL listed, SEE THE CURRENT DIGEST (Safety Switches ) FOR SPECIFIC CATALOG NUMBERS.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top